Part Number: SN65C1168E
Hello,
I am designing RS485 interface circuit.
I want to find out if the SN65C1168E can be used in a circuit with an RS485 interface.
Termination resistor of RS485 interface circuit is 120ohm X 2.
And VCC of SN65C1168E is 5V.
If Texas INstruments has an RS485 transceiver IC that is pin-compatible with the SN65C1168EPW and operates from +5V power supply, please let me know.
Regards,
MESH