This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65C1168E: Adoption for RS485 circuit

Part Number: SN65C1168E


Hello,

I am designing RS485 interface circuit.

I want to find out if the SN65C1168E can be used in a circuit with an RS485 interface.

Termination resistor of RS485 interface circuit is 120ohm X 2.

And VCC of SN65C1168E is 5V.

If Texas INstruments has an RS485 transceiver IC that is pin-compatible with the SN65C1168EPW and operates from +5V power supply, please let me know.

Regards,

MESH