Part Number: TUSB8041-Q1
Dear Expert,
Good day!
From the naming definition , the TUSB8041-Q1 should be auto-rating product , But from its datasheet
Its operate temp range is up to 85C , Tj up to 105C , normally the auto-rating device should up to 125C.
the ESD rating is only 2K (HBM) ,
It looks like a catalog rating device , could you help me to confirm is it the datasheet error ?
Thanks
BR,
Leon.liu