Can you tell me the difference between the SN55115J, J38510/10404BEA and J38510/10404BEB? Is the BEA an alternate for the BEB?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you tell me the difference between the SN55115J, J38510/10404BEA and J38510/10404BEB? Is the BEA an alternate for the BEB?
Matt,
Material wise they appear to be all same. But when looking up the test flow and reliability classification information, they have slightly different flow:
|
Orderable Device |
Rel Class |
Device Marking |
|
SN55115J |
MIL-COM |
SN55115J |
|
JM38510/10404BEA |
JANB |
JM38510/10404BEA |
I wasn't able to find information on the 10404/BEB, but my assumption is it is also a different reliability flow. Functionally, these devices should all behave the same.
Regards,
Eric Hackett