Other Parts Discussed in Thread: TCA9548A-Q1, TS3A5017-Q1, SN74LVC2G66-Q1, TCA9548A, PCA9518
Hello,
Customer was looking at the TCA9548A-Q1 for:
"I was trying to find a buffer with an enable such that I could set up an array of buffers and use them as a simple to control mux. I was getting concerned about the number of the buffers warning that one side could not have pullups on it or be connected in parallel to another buffer. The task I have is to test a device with 4 masters and simulate a I2C device on the other end. The lead wants them to be isolated from one another to avoid cross talk as there are shared addresses."
I am having trouble understanding the customer's design. Before I call the customer to learn more, I'd like to have some background knowledge. I couldn't find a similar application TI.com. Is anyone familiar with this design?
Any help would be greatly appreciated.
Best,
Alex