Hi team,
Could we set the ODLI output to D4-D7 when using dual link input and single OLDI output? Default is from the D0-D3 output.
Datasheet mentioned for replicate mode D4-D7 could copy the D0-D3 data, but could set the D4-D7 even not in replicate mode?
Thanks.
7.4.1.4 2-Lane FPD-Link III Input, Single Link OpenLDI Output
In this configuration the PCLK rate embedded within 2-lane FPD-Link III frame can range from 50 MHz to 192
MHz, resulting in a link rate of 875 Mbps (35 bit × 25 MHz) to 3.36 Gbps (35 bit × 96 MHz). Each LVDS data
lane will operate at a speed of 7 bits per LVDS clock cycle; resulting in a serial line rate of 350 Mbps to 1344
Mbps. CLK1 operates at the twice the rate as PCLK with a duty cycle ratio of 57:43.
7.4.1.5 1-Lane FPD-Link III Input, Single Link OpenLDI Output (Replicate)
Same as 1-lane FPD-Link III input, single-link OpenLDI output mode, and duplicates the LVDS signal on D4 to
D7 outputs.