This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD6S300A: Proper ESD protection device for USB 3.1 Gen2, DisplayPort 1.4

Part Number: TPD6S300A

Hello team,

I have received a question from my customer about the USB ESD protection device TPD6S300A.

My customer is searching for a device for the USB Type-C connector, and they listed TPD6S300A as an ESD protection device. so I want to check the specifications.

Is this device the proper ESD protection device for USB devices that meet the following criteria? If there are better device for this usage, we would like to know it.

  • USB 3.1 Gen2 (10Gbps)
  • DisplayPort 1.4(Alternate mode)

If there are more information needed about the customer's requirements, please contact us. 

Best Regards,

Ryotaro Fukui