Part Number: TUSB4020BI
HI,
Customers want to drive this device and other loads with USB bus power 500mA.
Looking at the power consumption of this device, USB 2.0 2 HS has VDD33 = 60mA and VDD11 = 80mA, so the current remaining in the load is 360mA.
Is this calculation correct?
They are considering replacing the Micro Chip: USB2514, but require a minimum of 400mA for the load.
Best regards,
Hiroshi