This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB4020BI: Power consumption

Part Number: TUSB4020BI


HI,

Customers want to drive this device and other loads with USB bus power 500mA.
Looking at the power consumption of this device, USB 2.0 2 HS has VDD33 = 60mA and VDD11 = 80mA, so the current remaining in the load is 360mA.

Is this calculation correct?

They are considering replacing the Micro Chip: USB2514, but require a minimum of 400mA for the load.

Best regards,

Hiroshi