Part Number: TCA9617A
Hello,
Can i use the TCA9617A in star connection as shown below. Each I2C slave with different address is working at 1MHz frequency.
Pull ups are provided at each slave. Little bit afraid of loading caused by 4 slaves on one output of TCA9617A.
Datasheet does say it can drive loads with 550pF or higher. What will be the max load it can drive for 1MHz ?

Thanks
ATharva