Part Number: SN65LVDM050-Q1
Other Parts Discussed in Thread: SN65LVDM050
Hi TI support,
I have a question regarding SN65LVDM050-Q1 part number.
Within its datasheet (i.e. SGLS128A − JULY 2002 − REVISED APRIL 2008), it is mentioned that the transceivers can run up to 500Mbps, with some power dissipation characteristics at 200MHz for Driver and Receiver.
We implemented this components for these characteristics on several of our boards.
I also did check the following technical documentation: . SLLS324J–DECEMBER 1998–REVISED JULY 2009 (for SN65LVDM050).
Same characteristics are given for the power dissipation at 200MHz (for both drivers and receivers), however: Table 1 shows that maximal data rate is equal to 100Mbps (-> 50MHz).
My question is the following: Shall I consider the same data rate for the SN65LVDM050-Q1? Or can you confirm that SN65LVDM050-Q1 is operating fine at 100MHz (i.e. 200Mbps)?
I do have some doubts since I do expect that both components are very similar.
Thank you in advance,
Marc