This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988EVM: Are better schematics available? Hard to discern what portions are needed for integration of the part

Part Number: TPS65988EVM


I am designing a product where we are only supporting 5V, a single DRP port, with a preferred UFP swap for data and supporting all swaps for power. There is no alternate modes supported, no USB 3.0, no BC, and am trying to determine which sections of the schematic are actually relevant. 

The schematics in the user guide for the EVM are blurry, for instance Figure 9-4 is largely illegible. Is it possible to receive the schematics separately?