Part Number: P82B715
Hello
I like to use the P82B715 on a PCB Device A which I design. Device B can be a version without P82B715 and with P82B715. Of course when I implement the P82B715 on both sides, It will work. But what happens if I have some devices on the I2C Bus without a P82B715 driver but the same voltage levels? Is this working and the noise immunity better then without the P82B715 on both sides? I have some sensors over a 5m cable with around 500pF and 50kHz I2C and getting some errors in the ciommunication sometimes. With the P82B715 this errors will be eliminated I hope, but I have still some sensors which I should support and without a P82B715 inmcluded.
Thanks for a reply, Dominik