Part Number: DS90UB941AS-Q1
Dear TI:
I want to know more about this bit's info.
1. 18B means color depth? Like RGB666?
2. If the stream input is configured to RGB888, then it's changed to RGB666 if this bit is set to '1'?
BRs,
Arvin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Dear TI:
I want to know more about this bit's info.
1. 18B means color depth? Like RGB666?
2. If the stream input is configured to RGB888, then it's changed to RGB666 if this bit is set to '1'?
BRs,
Arvin
Hello Arvin,
1) correct.
2) correct. In 18-bit mode, the 6 most significant bits (bits 7-2) of the Red, Green, and Blue outputs are enabled. The 2 least significant bits will be 0.