Hi team,
My customer is using UB949, and using GPIO0 as touch screen interrupt signal from serializer.
They set GPIO0 as Remote-hold mode or Remote-default mode to keep "no interrupt" state during link loss.
However, GPIO0 goes low when the serializer restart by PDB or some reason because the registers are reset to default.
Is there any way to avoid this situation?
If it cannot be solved by software, my customer have to think the solution by hardware. But it's really difficult situation due to the project schedule. Please consider a software solution.
BTW, I consider the false interrupt signal can be masked by HPD output like below. It need hardware change.
Could you check the feasibility? Is there any concern?

Best Regards,