Part Number: NS16C2552
Hi Team,
I have two questions.
1. Regarding the sampling operation with the internal counter at 16x clock.
Datasheet P32 "The sampling clock allows data to be sampled at the 6/16 to 7/16 point of each bit."
Is this done specifically at the rising or falling edge of the clock?
I imagine that the sampling is done in sync with the falling edge of the 6/16 clock.
2.The start bit is at the 8th clock as described in "At 8th 16X clock".
Why is there a difference between the data and the start bit?
"The RSR operation is described as follows.
1:At the falling edge of the start bit, an internal timer starts counting at 16X clock.
At 8th 16X clock,approximately the middle of the start bit, the logic level is sampled.
At the 8th 16X clock,approximately the middle of the start bit, the logic level is sampled.
if a logic 0 is detected the start bit is validated."
Regards,
Kenji