Part Number: TCA9511A
Other Parts Discussed in Thread: TCA4311A, TCA9617A
Hi team,
My customer evaluation TCA9511A and TCA4311A, and have some questions, please help me.
1、9511 and 4311 are hot-swappable chips. What is the main difference between them?
2、Sepc mentioned that 9511 and 4311 should have incremental offsets. Can they be directly interconnected? What impact will the direct interconnection have?
3、Can 9511 and 4311 be used as bus drive sources, similar to the function of TCA9617A. When evaluating the I2C bus load, only the bus load after 9617 needs to be calculated, instead of the wiring length before 9617? If so, what are their driving capabilities; if not, how do you understand the bus buffer mentioned in the spec?
There are many problems and the project is urgent. Please help answer as soon as possible. If you have any questions, please feel free to contact us. Thank you very much.
Best regards,
Andy Liu