Dears,
Customer ask
1. EVM said LFMODE LOW: 5 MHz ≤ PCLK < 15 MHz. HIGH: 15 MHz < PCLK ≤ 96 MHz
2. But Datasheet said LFMODE = 0, 15-MHz ≤ TxCLKOUT ≤ 96-MHz (Default) LFMODE = 1, 5-MHz ≤ TxCLKOUT < 15-MHz
Which one should be right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears,
Customer ask
1. EVM said LFMODE LOW: 5 MHz ≤ PCLK < 15 MHz. HIGH: 15 MHz < PCLK ≤ 96 MHz
2. But Datasheet said LFMODE = 0, 15-MHz ≤ TxCLKOUT ≤ 96-MHz (Default) LFMODE = 1, 5-MHz ≤ TxCLKOUT < 15-MHz
Which one should be right?
Hi,
The EVM users guide is saying that if the switch is low or high what LFMODE the device will be in, the datasheet is saying what the LFMODE mode will be in if the LFMODE's pin is a 1 or a 0, So they both are correct.
Regards,
Michael W.