Part Number: DP83826E
We use LED0 for the "link/activity" and LED1 to indicate the "10/100" speed.
DP83826E works in BASIC mode: can the function of LED1 on pin31 for 10/100 speed be set with Strap1 and also with register?
Which register should be used? Should I just set bit 3-0 of the LEDCFG Register (Address = 0x460) or are there other registers I should set?
I tried strap1 via pull-up resistor but it doesn't seem to work.
Pin description fuction in basic mode says: "Pin31 -Transmit errors: The pin acts as TX_ER as default. This pin can be configured to LED1 thru register configuration".
It does not say as in ENHANCED mode : "The pin can be configured to act as LED1 using strap or register configuration".
Do you have any suggestions?
Thank you for your help
Robert