Part Number: TPD4E001
Hi,
I am using the TPD4E001RDBVR for ESD protection of a USB signal. The board contains inrush limiting circuitry that sits between the 5V line of the USB bus and the 5V line powering the other board components, which functions to slow down the 5V rail during a plug-in event. I was wondering if there is any disadvantage to using this slower 5V rail for the ESD protection chip power? Or should I directly route the USB 5V connector pin to the power-supply input of the chip? In both cases a 0.1uF decoupling capacitor would be used to bypass the power-supply input to ground. I’ve included screenshots of the two schematic configurations below. U6 is the ESD chip.
Inrush limited supply:
Direct supply:
Thanks,
Colton Acosta