Part Number: DS160PR410
Hello Team,
I have a question about Power-On Default Equalization Configuration at I2C Slave Mode.
in documents(DS160PR410 Programming Guide) , default values are listed below.
- default value of reg_03 : 0x80
- default value of reg_04 : 0x16
It seems that the default values are not listed in the CTLE Index Table. (Table 8 of documents)
Q1. please tell me the CTLE Gain value corresponding to this default value. (xxx dB at 4GHz/ yyy dB at 8GHz)
Q2. Without ANY register modification after power on, which value of CTLE Gain?
Best Regards,