Part Number: DS80PCI402
Hello,
we are facing a power-up issue on a PCIe x4 link between mainboard and (FPGA based) PCIe add-in card where the DS80PCI402 is used as Re-Driver between mainboard slot and card slot (link is not getting established or in x1 only instead of x4).
The issue is (or seems to be) solved if we set the DS80PCI402 RXDET to Manual-Always-ON mode (by 1K pullup on the RXDET device pin).
Are there any drawbacks/disadvantages using this mode in systems where the actual add-in card may be a x1 card at some times and an x4 card at other times (this is not a battery powered system)?
What's the point about the receiver detection phase (LTSSM DETECT state) anyway? Isn't this all determined later on in the LTSSM POLLING/CONFIGURATION states?
Thank you.