This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD1E0B04: USB2.0 DN/DP Line?

Part Number: TPD1E0B04
Other Parts Discussed in Thread: ESD122, TPD1E04U04, TPD1E01B04

Hi,

Please see below customer question:

I reviewed TI TVS diode to use USB2.0 DN/DP line.

Part Number : TPD1E0B04DPLR  X2SON-2

Can it use USB2.0 DN/DP line? 

Why I review the this part, I can’t find that have Low capacitance and small (0603 mm) size TVS.

Similar item TPD1E0B04DPLR datasheet in TI, you recommend  DP/DN Line voltage value 0V to 5V.

If we use only DP/DN lines(Do not use control line), Can I use  TPD1E0B04DPLR Item?

(As I know DP/DN Voltage level lower than 3.6V.)  

 Thanks,

Antonio