This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: If the DOUT1+/- pin can connect to a DC voltage through the AC cap?

Part Number: DS90UB947-Q1


Hi, Team:

Can you help to check if 947 or 941's DOUT1+/- pin can connect to a 12V DC voltage through the AC cap?

The background is in last generation, customer use 948 port0 to transfer the video and port 1 in connector are used to transfer the power. when the display connect to dual output 941/7 system, 941/7 Dout1+/- will connect to the 12V through the AC couple cap.