Part Number: TCAN1042HGV
Hi
Can TCAN1042HGDR replace TCAN1042HGVDRQ1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
The Q100 rated devices are tested and qualified under the AEC 100 standard to ensure quality and robustness in safety critical applications. Devices labeled with the "-Q1" suffix have undergone additional testing to ensure they meet the requirements for demanding end applications such as automotive systems. Non-Q1 rated devices do not have significant differences to those that qualify for the Q100 rating, but they forego the extra testing so compliance to this standard cannot be guaranteed.
If the Q100 qualification is not required by the EOM, a non-Q1 device can be used in place of an unavailable Q1.
Let me know if you have any more questions.
Regards,
Eric Schott
Hi Gareth,
The 'V' suffix indicates that the device supports internal logic level translation using pin 5 (Vio). For non-V devices, this pin is a NC. If the voltage translation is not needed (Vio = Vcc), or translation is done externally, a non-V device can replace a V variant. If the swapping the other way, Vio should be connected to Vcc.
Regards,
Eric Schott