Part Number: MAX3243E
Hello Sir,
As datasheet mention in auto-powerdown mode, the driver will disable if no valid signal at at RX_IN.
So we can't to do loop-back test (TX_OUT connect to RX_IN) when hardware configure as auto-powerdown mode (FORCEON= LOW, FORCEOFF=HIGH) right?
Two device can't communicate if both hardware configure as auto-powerdown mode (FORCEON= LOW, FORCEOFF=HIGH) right?
Is that mean, auto-powerdown mode transceiver only can communicate with without auto-powerdown transceiver otherwise will not workable?
Looking forward your comment. Thanks!!