Part Number: TPD4E001
Other Parts Discussed in Thread: TPD4E1U06
Hi team,
is 0.1uF bypass cap must to have at pin5? Thx.
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andrew,
As mentioned in the datasheet design recommendations, Section 8.2.2, it is highly recommended to connect a 0.1uF bypass capacitor on the supply pin close to the device.
Thank you,
Regards,
Sandesh
Hi Andrew,
To follow up on Sandesh's point, while the 0.1 uF cap is recommended, it is not absolutely required for the device to function. The additional capacitor is just there to give you additional protection on the Vcc line. However, if you want a device that does not have a Vcc line and doesn't require an additional capacitor, I would recommend a device like TPD4E1U06.
Regards,
Matt Smith