Part Number: DP83822IF
Hi team,
My customer reported an issue with DP83822IF. The device is operated in 100BASE-FX mode. The problem is in sometime once the link dropped due to the fiber cable is disconnected, the link cannot recover automatically once the fiber is connected again until the PHY is reset.
I noted there is a NOTE in datasheet, it says "... if the electrical link between the fiber module and the DP83822 is broken, disconnected or otherwise disrupted, the link will recover only by initiating a soft
reset through MDIO/MDC interface."
I am not sure if this is the root cause of my customer's issue? If disconnection of the fiber cable results 'DISRUPTED' of the electrical link (between fiber module and the DP83822)?
Thank you!
John