This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: Measures to optimize radiated susceptibility

Genius 17485 points

Part Number: DP83826E

Hi all

My customer is using the DP83826ERHBR.

During the radiated susceptibility tests at 10V/m they lost the ethernet communication with the DP83826ERHBR (acceptance criteria A).

This was for frequencies in the 1.3 – 1.6 GHz range.

What are the critical points to watch out for to improve the susceptibility to radiated emissions ?

Please comment and point to helpful collateral.

Thank you and best regards

Ueli