Part Number: TLK2711-SP
hi,
I havent saw any detailed info on TLK2711A on this but there was more info on TLK2711-SP:
my plan is never use the RX and only use the device as transmitter only.
this is why I plan tie the LCKREFN to pull down resistor to ground.
when powering up the device, even though I dont want to use the RX, do I need to assert high the LCKREFN and after power up completed a few milisec after place it in constant "0"?
similar question to ENABLE pin, in powerup diagram of the TLK2711-SP (I am using TLK2711A, but still...) it seems that ENABLE need to be "1" prior to power up the supplies (same as LCKREFN).
is this a must?
will the device work correctly if ENABLE is low during power up and only when I want to transmit data through TXD->DOUT I can set the ENABLE to "1"?
will the device work correctly if LCKREFN is low during power up and stay low all the time?