Part Number: HD3SS3220
Hi teams
There are two device using HD3SS3220 and setting to DRP in GPIO mode.
At first step, they connect then who will be DFP, how do they decide their role?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DRP devices will initially toggle their state between DFP (by connecting Rp and disconnecting Rd ) and UFP (by disconnecting Rp and connecting Rd ) operation, until the complimentary termination is found at the port partner on one of the CC lines.
When two DRPs are connected together, they accept the resulting DFP-to-UFP relationship achieved randomly. Both DRPs toggle their states between DFP and UFP . Whenever a successful Rp – Rd voltage divider is formed on one of the CC lines, the connection is established.
Hi Brian
Is stand process of two DRP depending on who provide the power and then the one will be DFP?
And your above mentioned the achieved randomly scenario is for all of both sides could provide power?
Eddie:
As DRP , they both should provide power when configured as DFP. But Vbus is not requirement during CC configuration to decide which is DFP or UFP
Regards,
Brian