Part Number: TPS65987DJEVM
Other Parts Discussed in Thread: TPS65987D
Hello,
We are currently using the TPS65987DJEVM to generate a flash that can be programmed directly to the TPS65987D via a MCU. We need to source 9V (preferred but not required) given an input of 5V. First, is this possible? If so, does the EVM need an external adapter such as Aardvark or the FTDI for flashing? We have attempted to flash the EVM through J3 and with all the switches on, but the application customization is unable to detect an address. Please let us know how to fix these problems, thanks!