Part Number: TRS3122E
Hi,
1.Data rate support 1000kbps in the TRS3122E Datasheet(RL=3k ohm & CL=500pF)
How should the circuit be added the RL and CL?
2.The transmission speed we currently use is 115200bps. Is there a limit on the transmission length?
If I want to use 1000kbps, is there a limit on the transmission length?
3. Is there a way to reach 1000kbps with 2 wires (Tx & Rx) alone and I can't lose data? Do I need to change to 4 wires HW flow control (CTS & RTS)?
If it needs to be changed to 4-wire, is there a way for this (TRS3122E) to achieve the 4-wire configuration (that is, the second group is changed to CTS & RTS)?
If it can't be achieved, can you recommend one that can be achieved?
Thanks.
Patrick