Part Number: DP83867E
Dear Expert .
Good day!
Our customer are planning to use the DP83867 PHY and want to use the RX recovered clock from the device to be the master clock input into an FPGA using the CLK_OUT from the PHY to be able to run the FPGA synchronously with the recovered clock. Can you provide information on how the CLK_OUT works when programmed for outputting the RX_CLK and set for 100 Mbps operation with 25 MHz CLK_OUT frequency? For instance,
1. What is on the CLK_OUT pin when the Ethernet link is not set up yet? Is the CLK_OUT a free running 25Mhz signal in that case?
2. What happens to the CLK_OUT when the link is up and the recovered RX clock is available? Does the CLK_OUT become synchronous with the recovered clock and is it a graceful switchover?
BR,
Leon.liu