We bought two number of the DP83TG720EVM. We would like to set the test mode using USB interface.
Can you give details about setting the test mode for this board.
Ramesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We bought two number of the DP83TG720EVM. We would like to set the test mode using USB interface.
Can you give details about setting the test mode for this board.
Ramesh
Hello Rmaesh,
Thank you for the query.
Please refer to the below documents and the EVM use guide.
https://www.ti.com/lit/pdf/snla371
Please refer to 7.3.1.3.3 Programming Datapath BIST section of the data sheet.
What test are you looking to configure ?
Regards,
Sreenivasa
Hi
Thanks for the document, it seems we need to program the register manually to do it. There are pre requisite as well that I need to program register set based on Master or in slave mode. Do you any utility that can be used to set the test mode directly .
Ramesh
Hello Ramesh,
Thank you for the mail.
You can use the UBB2MDIO utility and write some simple scripts.
Regards,
Sreenivasa