Part Number: TLK106L
Other Parts Discussed in Thread: TLK105L, , TLK106
I had a question on the TLK106L. I’m using the TLK106 PHY chip on my board .The datasheet is generic , and also applies for TLK105L.
The TLK106L works at maximum temperature of 105 °, while The TLK105L works at maximum temperature of 85°. if I guarantee a lower working temperature,
can I consider them to all intents and purposes compatible with each other?
Thanks