Dear team,
The customer plans to use 941's splitter mode to drive two 1920*720@60fps display. The horizontal blanking is 160, and the vertical blanking is 40, so the display PCLK=(1920+160)*(720+40)*60=94.848MHz. For our 941, we use splitter mode, so we only use one DSI port. Our one port can support 105MHz, but the two display's PCLK is 94.848*2=189.696MHz. One port of 941 can't support so large PCLK, so we can't support two 1920*720@60fps display with splitter mode, right?
Thanks & Best Regards,
Sherry