Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB913A-Q1, DS90UB933-Q1
Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I am using ov10650 connected to serializer UB953 linked to my UB960 and at the end, i would like to recover video from the camera on a µprocessor (IMX8M Mini). I developped a driver in order to use the serdes camera but I am facing a last issue concerning the data format of the video.
The OV10650 outputs RAW12 format. When connected to 953 ser and 960 des (in mipi csi-2 synchronous mode), which is the format transfered at the output of the DES? Is it still RAW12 ? or another one like YUV... I am asking this because I saw somewhere that MIPI CSI-2 couldn't get RAW format but I still can get camera video as CSI-2 data at the output of the DES (saw on oscilloscope). Can i program the desired output format at the DES ? WHich settings do I need to put on the DES? "RAW12" as input data from the SER?
Regards,
Danilo