Part Number: TUSB3410
Hello,
I used linux 4.18 and already enabled ti_usb_3410_5052 dirver.
But I still got error dmesg "Direct firmware load for ti_usb-v0451-p3410.fw failed with error -2" when pluged micro usb to USB port.
Config and fail log like attach file.
Linux version confirm: #uname -a Linux localhost.localdomain 4.18.0-193.el8.x86_64 #1 SMP Fri May 8 10:59:10 UTC 2020 x86_64 x86_64 x86_64 GNU/Linux #cat /proc/version Linux version 4.18.0-193.el8.x86_64 (mockbuild@kbuilder.bsys.centos.org) (gcc version 8.3.1 20191121 (Red Hat 8.3.1-5) (GCC)) #1 SMP Fri May 8 10:59:10 UTC 2020 driver confirm: #lsmod |grep -i usb ti_usb_3410_5052 32768 0 usbnet 49152 1 cdc_ether mii 16384 1 usbnet usb_storage 73728 2 uas Error dmesg after plug micro USB to USB. #dmesg 2oj4[22379.280681] usb 1-2: new full-speed USB device number 17 using xhci_hcd [22379.429139] usb 1-2: New USB device found, idVendor=0451, idProduct=3410, bcdDevice= 1.00 [22379.429144] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [22379.429147] usb 1-2: Product: TUSB3410 Boot Device [22379.429149] usb 1-2: Manufacturer: Texas Instruments [22379.429151] usb 1-2: SerialNumber: TUSB3410 [22379.432705] ti_usb_3410_5052 1-2:1.0: TI USB 3410 1 port adapter converter detected [22379.433070] usb 1-2: Direct firmware load for ti_usb-v0451-p3410.fw failed with error -2 [22380.019290] usb 1-2: reset full-speed USB device number 17 using xhci_hcd [22380.151914] usb 1-2: device firmware changed [22380.152082] usb 1-2: USB disconnect, device number 17 [22380.266650] usb 1-2: new full-speed USB device number 18 using xhci_hcd [22380.441195] usb 1-2: New USB device found, idVendor=0451, idProduct=3410, bcdDevice= 1.00 [22380.441200] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3 [22380.441203] usb 1-2: Product: TUSB3410 Boot Device [22380.441205] usb 1-2: Manufacturer: Texas Instruments [22380.441208] usb 1-2: SerialNumber: TUSB3410 [22380.444113] ti_usb_3410_5052 1-2:1.0: TI USB 3410 1 port adapter converter detected [22380.448216] ti_usb_3410_5052 1-2:2.0: TI USB 3410 1 port adapter converter detected [22380.448740] usb 1-2: TI USB 3410 1 port adapter converter now attached to ttyUSB0 [22394.322627] sr 14:0:0:0: [sr0] CDROM not ready. Make sure there is a disc in the drive. [22394.327675] sr 14:0:0:0: [sr0] CDROM not ready. Make sure there is a disc in the drive. [22394.334265] sr 14:0:0:1: [sr1] CDROM not ready. Make sure there is a disc in the drive. [22394.340303] sr 14:0:0:1: [sr1] CDROM not ready. Make sure there is a disc in the drive.
Could someone help me to this problem?
Thank you so much.