This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB542: Inquiries about the application circuit

Guru 12705 points

Part Number: TUSB542

Hello,

My customer has some questions about the following TUSB542 application circuit in the TUSB542 datasheet.

The customer thinks this is a float setting when using a 4.7k pull-up/donw resistor on the B2 pin. Is that correct?

Why is the 4.7kohm pull-up/down register used only for B2 pin among the CNFG pins?

Thank you.

JH

  • JH

    The connections for CNFG pins of TUSB542 is example only.

    Refer to Table 2 and section 6.6 Electrical Characteristics, DC, floating voltage means VCC/2. So having both pullup and pulldown resistor will result in VCC/2 -> Floating.

    It is recommended to run an overall system signal integrity analysis, in order to estimate the channel loss and configure the re-driver. It is also recommended to have pull-up and pull-down option on all the configuration pins for debug and testing purposes.

    Thanks

    David