Part Number: DS90UB962-Q1
Dear:
i want to know whether DS90UB962 can support 4 channel 2M 30fps or 1 channel 8M 30fps ? because I want to connect eight millions of pixels sensor, can you help me promote which deserializer and serializer solutions ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB962-Q1
Dear:
i want to know whether DS90UB962 can support 4 channel 2M 30fps or 1 channel 8M 30fps ? because I want to connect eight millions of pixels sensor, can you help me promote which deserializer and serializer solutions ?
Hi Cooper,
The 962 can fully support 2M imagers, so 4x 953 2M imagers should work as long as CSI-2 aggregation input/output bandwidth constraints are followed (output less than output bandwidth).
In some cases 8M at 30fps is feasible, but depends on the bits per pixel, resolution, etc.
For further options using roadmap or non-public devices, please reach out to your local FAE support for more information.
Regards,
Logan
Dear Logan:
thanks for your feedback, you mentioned CSI-2 aggregation input/output bandwidth constraints are followed (output less than output bandwidth),the mean is output less than input bandwidth,right?
Hi Cooper,
Output bandwidth needs to be greater than input bandwidth; sorry for that typo.
More information regarding CSI-2 aggregation can be found in the CSI-2 Aggregation Breakdown video on the FPD-Link learning center.
Regards,
Logan