Part Number: DP83869HM
Other Parts Discussed in Thread: THS4551, , DP83869
Hi Team,
Customer want to drive SIP & SIN pins and the input for these pins are from THS4551. Please refer below image, the Differential output from THS4551, obtained from PSpice Simulation. The same output is given as input to DP83869HM, at SIP & SIN pins.

So, is this a valid input to DP83869 chip ?
As per the 8.5 : Electrical Characteristics of datasheet, which says 350mV is the min Voltage.
Output Voltage from THS4551 is 400mVpp, the worst case is 150mVpp.
Can DP83869 work on this voltage levels.
Regards, Shinu.