Part Number: DS80PCI800
Other Parts Discussed in Thread: DS80PCI810
Hi team,
We are designing DS80PCI800 in INTEL's Sandy Bridge platform but we would like to confirm below two questions.
1. Is DS80PCI800 designed ok in below Sandy Bridge platform's convert board?
2. Is there any trace length limited between CPU and Redriver & between Redriver and PCIE device?
We use that CPU‘s PCIEX8 connect user encryption card directly , X8 bandwidth is normal;
but convert board use DS80PCI800(one TX,another RX),the encryption card about 8 inches away from the RX side, final parameters of TX/Rx's eight channels are EQ=0x07,VOD=1.4V,DEM=-1.5dB; now X8 bandwidth could be X1 or X2 or X4!
We do not know how to adjust these parameters to meet x8 bandwidth normal。Please help us!
Thanks