Part Number: DP83TC812S-Q1
Hi Team,
My customer is looking to connect 2 ECUs via ethernet and they have a spec that shows the two ECUs could have a ground shift differential of up to 2V when comparing one to the other.
With this, can you clarify if either of the two situations are of any concern:
1. There is a DC 2V difference between grounds of two connected Phys
2. During operation there is a transient 2V ground differential (only for a few us/ms) between the two Phys.
If this is covered by an ISO ethernet specification, any information about that would be helpful.
Best,
David