Part Number: NS16C2552
Dear Specialists,
My customer is evaluating NS16C2552 and has questions.
I would be grateful if you could advise.
---
According to the data sheet
UART reception has an internal sampling clock that is 16 times the data rate and
This sampling clock states that the data is sampling at 6/16 to 7/16 points of each bit.
We use data: 8bit, start bit: 1bit, stop bit 1bit, and parity for a total of 11bit.
Assuming that the sampling point deviates from the nominal sample point by 0.5ΔT, if this data is received continuously for 4 bytes,
1) Resynchronize the sampling clock for each start bit
→ Max deviation is (11-0.5) x ΔT
2) Synchronize the sampling clock only for the first start bit
→ The deviation of max is (44-0.5) x ΔT
Which one will it be?
Is your answer the same for PC16552.
---
I appreciate your great help in advance.
Best regards,
Shinichi