Part Number: NS16C2552
Dear Specialists,
My customer is considering NS16C2552 and has a question.
I would be grateful if you could advise.
---
About NS16C2552
(1)Is a 2kΩ pull-up required when using an external oscillator?
Is it the same for PC16552?
(2) Regarding NS16C2552,Oscillation frequency; 18.432MH has been confirmed,
The rising edge of the oscillation waveform rises quickly, but the falling waveform is gentle.
I am checking the falling waveform.
In the case of such a waveform, it is expected that it is used in a situation where the DYTY ratio varies.
Is there a possibility that communication will be poor if the sampling shifts little by little?
Is there a standard for duty ratio?
If there is a duty ratio standard, is it the same for PC16552?
---
I appreciate your great help in advance.
Best regards,
Shinichi