This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Design of thermo electric cooler for laser diode

I want to design thermo electric cooler for laser diode with following specification
We are design house and reference designs will make our job easy
• Thermistor sensor input
• 900 Hz Base Frequency Pulse Modulated Output
• Heat, Cool or H-Bridge operating modes
Red LED Heating Mode
Green LED Cooling Mode
• PID control, parameters set
• Optional High and Low Alarm Settings
• Optional Remote LED Display
• Optional Remote Set Potentiometers
• Proportional Integral Control Algorithm
• TTL to USB communication via Optional Cable
• Input Voltage: 6 to 28 VDC
• Output Voltage: 0 to 28 VDC
• Load Current: 0.1 to 12.5 A
• Temperature Resolution: 0.01°C
• Control Stability: ± 0.1°C
• PID Functions:
o Bandwidth : 0.1 to 55°C
o Integral: 0 to 10 repeats per minute
o Derivative: 0 to 10 minutes
• Ambient Temperature range: -40 to 250°C
• 450 W Output Power Control
• Bidirectional load rating: 12.5 AMP max
• Dual power supply to separate load and logic
please share details of components used with data sheet application note