Part Number: TPS25830-Q1
Other Parts Discussed in Thread: TPS25831-Q1
Hello,
My customer is considering using TPS25830-Q1 without using DM/DP pins. In the system DM/DP pins of the connector will be shorted with 200mohm; therefore, the port will be recognized as BC1.2. TPS25830 is configured as both CTRL1 and 2 are 1. Do you think CC1/CC2 control works properly and the DCDC convertor supplies the BC1.2 current?
By the way, TPS25831-Q1 cannot be considered, because why the customer came up with this idea is because of its current tight supply.
Thanks!
Regards,
Oguri