This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: can it support 1080p60 with deserializer ds90ub940

Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: DS90UB940N-Q1, DS90UB948-Q1

Hi Experts,

I'm trying to bring up DS90UB941 and DS90UB940. 941 is used to serialize MIPI DSI and 940 is used to deserialize it.

For now, ds90ub940 has worked successfully with resolution 720p60. 

On page 133 in 941's datasheet, "The DS90UB941AS-Q1 can support up to 170MHz pixel clock when paired with DS90UB940N-Q1 , and up to 192MHz pixel clock when paired with a DS90UB948-Q1." 

But I tried 1080p60. It failed. And as described in datasheet Page 1, the maximum pixel clock for single FPD-LINK is 105Mhz. Pixel clock of 1080p60 is 2200x1125x60=148500000. It exceeds the 105Mhz.

Could you help to confirm that the maximum resolution and frame rate of DS90UB941 when it works at single FPD-LINK?

Thanks very much.

 

Best regards,

Justin Ding