Part Number: AM26LV32
Hello,
I would like to know if this device will behave as expected if instead of a differential signal, a single-ended signal is supplied on the "A" input while the "B" input is left floating. This device is being used on a motor-controller board to accommodate differential Hall signals from an encoder. However, some encoder only supply single-ended Hall signals, so it would be nice if the same receiver can be used for both signal types. Since the A and B inputs are internally biased it seems to me that floating the B input is OK so long as the VIT+ and VIT- specifications are met. If B cannot be left floating, should it be pulled up or down and by what resistor value?
Thanks,
Narek